Mission Critical Communications (MCX)

전단지

The flyer for MCX (Mission Critical Communication) describes that MCX consists of voice (MCPTT) MC-Data and MC-Video. It describes why MCX is important, and in which sectors it will be used. The various types of MCX devices are described as well as the importance for the devices to be compliant to the 3GPP specs. The evolution of MCX in 3GPP is described and finally the support of MCX in S8704A Protocol Conformance Toolset.