Complete-End-to-End-Private-Network-Visibility

솔루션 개요

The Private 5G market is still in the early stages of enterprise and industry 4.0 deployments. Most production deployments are single-vendor solutions deployed in ports, transportation, and mining, with limited 5G requirements, for example addressing WiFi shortfalls and handover issues. As Private 5G deployments advance toward 5G’s more disruptive features (high capacity, wireless flexibility, and lowlatency performance) to deliver factory automation and immersive experiences, reliable and time-sensitive networks with stringent SLAs will be required.

As advanced Private 5G networks become operational, multi-vendor, best-of-breed networks, with end-toend assurance and security, will be critical to success. A key challenge will be interoperability pre-testing and ongoing performance visibility from devices, RAN or Open RAN, the standalone core, transport network, and edge platform.