백서
Network Modeling and Simulation in the Autonomous Car Era
The global autonomous vehicle market is valued at an estimated $54 billion—and is projected to grow tenfold in the next seven years.
Driverless cars, which navigate without input from their passengers, represent the next stage in design evolution.
But these vehicles will only be as safe, reliable and efficient as the communications supporting them.
Network modeling and simulation offer advanced and highly effective testing for these critical and sensitive communications networks.
Here we look at the use of network modeling and simulation technologies in the driverless car era.
무엇을 찾고 있습니까?