백서
Introduction
As organizations seek to walk the networking tightrope between the demands of performance management and network investment, they clearly need something to hang on to, to help them keep their balance. Mature enterprises are increasingly turning to network visibility as that proverbial balancing pole.
Without visibility, it is difficult to manage operational variables to maintain high levels of network performance—and it is nearly impossible to understand the threats maligning the network in order to maintain security and control over network assets. But simply throwing money at network and security monitoring tools does not provide the kind of visibility necessary to balance performance and control. Organizations also need to employ best practices to ensure they are getting the most out of their network and security monitoring investments.
The following five-step approach can help IT keep its balance while gaining that crucial visibility into the network.
Without visibility, it is difficult to manage operational variables to maintain high levels of network performance.
무엇을 찾고 있습니까?