New 6G Challenges Inspire Cross-Disciplinary Innovation

白書

Roger Nichols remembers sending his first e-mail using wireless networks in the early 1990s, from the back of a bus during his daily commute. That was 30 years ago, on a 1G network—at a data rate about fifteen thousand times slower than today. Now the 6G program manager at Keysight Technologies, Nichols sees the rapid growth of the current mobile wireless standard and knows that there is much more to come. As of June 2022, the Global Mobile Suppliers Association counted nearly 500 operators in 145 countries that had deployed—or planned to deploy—5G capabilities, up from 412 at the end of 2020. Omdia and 5G Americas project that by the end of 2022, more than 1.3 billion connections will be made to global 5G networks.