eBooks
Since 2015, many companies have been transitioning from semi-annually or quarterly releases to weekly, daily, and even releases by the minute.
Organizations such as Amazon release software roughly every 15 seconds. Mobile Apps are released to their Mobile App Stores at the rate of 1,000 per day.
Applications that were once built to be monolithic are becoming technology stacks that integrate many different pieces of software that perform different functions. In fact, Netflix has a technology stack of over 42 separate applications.
Legacy automated testing tools built for architectures from over 10 years ago cannot keep up.
Built originally for a limited set of technologies and the waterfall methodology, these tools, instead of being re-architected from the ground up, have simply had new features bolted on just to stay relevant.
何をお探しですか?