白書
Security is now a boardroom topic for every business. It has become one of the most important areas of executive concern because of its ability to:
At the same time, how do you translate these goals into a realistic and achievable security architecture? Inline security solutions are one way that organizations can address this question. The solution is more than just adding an inline security appliance, like an intrusion protection system (IPS) or a web application firewall (WAF). It requires complete data visibility, which allows examination of all data for suspect network traffic.
This white paper does the following:
Inline Security Market Drivers
According to the latest World Economic Forum report on global risks, cyberattacks and data fraud or theft are two of the top five risks that CEOs face 1 . This has led to a reprioritization of enterprise objectives and spending. Data from Forrester Research shows that businesses’ top security priorities for the next 12 months following January 2019 2.
何をお探しですか?