LTE / LTE-Advanced RF Measurements with the UXM Wireless Test Set

アプリケーションノート

The third-generation partnership project (3GPP) defines standards for development and test of 3G and 4G system components. The technical specification (TS) 36.521-1 defines requirements for radio frequency (RF) testing of long-term evolution (LTE) and LTEAdvanced (LTE-A) user equipment (UE). This application note provides example test procedures for RF testing of LTE and LTE-A UEs based on 3GPP TS 36.521-1 V12.2.0 (2014-06).

Many references are made to 3GPP TS 36.521-1 in this application note. In most cases, these references are abbreviated as 36.521. References to other 3GPP documents are abbreviated in a similar manner.

3GPP requires all tests to be performed over all E-UTRA bands supported by the UE. In some cases, there are band-specific setups and requirements. This application note provides example test procedures for frequency division duplex (FDD) E-UTRA Band 3. Additional bands can be tested following a similar set of steps. E-UTRA bands are defined in 36.521-1 clause 5.