アプリケーションノート
The backbone of Industry 4.0 applications is machine to machine communication. Transportation of information between machines and systems or machines to machines enables decentralized decision making. The challenge with machine-to-machine communication is that there was no standard “language”, each machine had its own communication protocols. IPC-CFX is an electronics manufacturing industry developed standard to address this challenge. IPC-CFX simplifies and standardizes machine to machine communication while also facilitating machine to business/business to machine solutions.
Keysight’s i3070 In-Circuit test system supports IPC-CFX, as well as other communication protocols such as MQTT, OPC-UA and Panasonic’s iLNB.
何をお探しですか?