eBooks
High Current Devices Add Complexity
Higher current devices typically include control logic, wiring, and fixturing that need to perform well when combined into a system. Reactive components create dynamic current spikes that are much larger than the already high steady state current. These current spikes can cause serious damage to your device. To understand your power and measurement needs, it is helpful to look at each part of a system.
何をお探しですか?