Case Studies
One of the major gaps in Indian Engineering is that while the number of engineering colleges are plenty, the number of employable degreed graduates is not. What has become clear is that due to old curriculum, lack of practical knowledge and limited technology exposure, industry expectations for industry-ready students are not always met. Industry and academia are working to bridge the gap between degree and employability, but these efforts are typically limited to just a few select institutes, depriving students from other colleges in India of good quality research and jobs.
PSG College of Technology in Coimbatore, India — established in 1951 and offering a total of 48 full-time and part-time programs in Science, Engineering, and Management — recognized this challenge and set out to minimize the gap. Its goal was to create an innovative learning environment and increase student exposure to industry. For help in achieving these goals it turned to Keysight Technologies. Keysight had previously engaged with PSG Tech on engineering curriculum, as well as a range of technology and measurement workshops.
Identifying A Need
Telecom is one of the fastest growing sectors in India with an acute shortage of skilled workforce. With multiple government initiatives underway and increasing demand for RF and microwave engineers, PSG Tech wanted to find a way for its students to learn the skills they needed to work competently in this high-tech arena.
To solve this challenge, PSG Tech and Keysight decided to establish Center of Excellence (CoE) labs on embedded and advanced wireless communications (Figure 1). As part of the school’s ECE department, the labs would provide students a hands-on learning experience with industry-grade software and instruments. The idea was that the labs would be manually set up, depending on specific technology and measurement needs, as well as industry requirements.
Innovating Engineering Education
PSG Tech’s first CoE lab focused on baseband communications and advanced embedded systems. The lab was equipped with Keysight’s industry-standard test and measurement instruments and industry-leading software measurement tools. Multiple test benches were set up to cater to students needs on 1:2 basis (number of test benches: number of students). This provided students an ample amount of time to work on the instruments and also learn the practical aspects of technology and measurement science.
With a mix of Keysight instruments that included mixed signal oscilloscopes, logic analyzers, digital multimeters, power supplies, data acquisition systems, and function generators, the faculty at PSG Tech was able to customize the lab for various applications, such as as automotive electronics, medical electronics, embedded systems, industrial instrumentation, sensor development, FPGA debug, and a host of serial protocols like CAN/LIN, RS232/UART, I²C/SPI, MIL-STD 1553/ARINC 429, and I²S. Best of all, once the CoE lab was established, it paved the way for other departments to collaborate with the ECE department on learning and design, development, and validation of technologies in the automotive, medical electronics, and robotics fields, among others (Figure 2).
One of the unique concepts implemented in the CoE lab was remote accessibility through the intranet/internet. Thanks to Keysight’s LXI compliance feature, most of the lab’s test equipment was easily connected to the LAN with a built-in web server. This provided both faculty and students the ability to access the lab anytime, anywhere without having to physically go into the lab.
何をお探しですか?