E7770A Common Interface Unit

データシート

 Definitions and Conditions

The Common Interface Unit (CIU) will meet its specifications when:

  • The CIU is within its calibration cycle
  • The CIU has been stored at an ambient temperature within the allowed operating range for at least two hours before being turned on; if it had previously been stored at a temperature range inside the allowed storage range, but outside the allowed operating range
  • The CIU has been turned on for at least 30 minutes

Nominal

Nominal values indicate expected performance, or describe product performance that is useful in the application of the product, but are not covered by the product warranty.