AWG Functional Building Blocks

白書

Arbitrary waveform generators (AWGs) are the most versatile signal generators available. An AWG can generate any mathematically-characterized signal, including sine wave, pulse, modulated, multitone, polarized, and rotated signals. As far as test equipment goes, the AWG is commonly viewed as a workhorse and can perform the functions of any other generator type. A typical block diagram of an AWG is shown below. The signal flow through the functional blocks starts with a numeric description of a waveform stored in memory. Then the selected waveform samples are sent to a digital-to-analog converter (DAC), filtered, conditioned, amplified, and output as an analog waveform.