Optimize Wireless Designs in Less Time

アプリケーションノート

The lifecycle of a wireless system, subsystem or component is very complex. To enable successful characterization, a signal analyzer must be able to test the limits of a design and validate compliance to the corresponding wireless standards. It is important to ensure that every wireless design meets or exceeds the relevant standards because testing to exceed compliance helps ensure reduced error margins and higher production yields. This can be accomplished with a midrange signal analyzer that is optimized to provide the best possible performance. Testing is easier with the latest signal analyzers that now include a streamlined, touch-based user interface (UI) that minimizes the time spent learning how to set up measurements and thereby creates more time to focus on design optimization. This application brief illustrates those benefits using the Keysight N9020B MXA signal analyzer. With its multi-touch UI, advanced software tools and modulation analysis, the MXA can help you resolve design issues in less time, enabling you to deliver new products to market sooner.