Programming the PXI Vector Network Analyzers (VNAs)

アプリケーションノート

This application note is intended to accompany the M937xA configuration guide and is written to assist software test developers and application engineers in the creation of an effective system integration for the M937xA PXIe vector network analyzer (VNA). This application note walks you through the process of developing a C# application using the IVI driver as the programming remote interface.

Using this application note will enable faster test development with the PXI VNA, resulting in lower initial test development cost and shorter time. It is assumed that the reader will be familiar with the fundamentals of programming in a COM and .NET development environment.