Coupling Two Signals on a Two-channel Waveform Generator

アプリケーションノート

It can be challenging for engineers to couple two signals together with a phase, amplitude or frequency relation. They need to ensure that if the parameter changes it changes on both signals. While the two signals by themselves might be simple, the act of keeping track of both of them is incredibly tedious. Dual-channel Trueform waveform generators now make keeping track of two signals much simpler. Using these waveform generators, coupling your signals together has never been easier or more accurate.