Managing Radar System Test with Radar Signal Simulation Solution

アプリケーションノート

As modern radar system accuracy requirements become more advanced, development and validation of such systems is increasingly challenging. What were once basic radar system test concepts have become very sophisticated in order to address the challenging scenarios supported by modern systems. This application note describes the challenges of radar test, and discusses of the benefits of a radar signal simulation test solution based on the advanced features of a highperformance PXIe arbitrary waveform generator. radio astronomy.

 

Radar system measurement challenges

While there are many elements of radar systems which contribute to system complexity, one aspect that creates a particular test challenge stems from the number of important functions of a radar system that are time-dependent.