TC611 Diode Model

技術概要

 Description

This product note provides a Spice model and a Libra model of the TC611 discrete beam lead GaAs diode. This diode is a modified barrier Schottky diode which features very low forward voltage and a soft reverse breakdown characteristic. The forward characteristics are modeled using a standard diode model (DMOD1). The reverse characteristics are best modeled using an anti parallel diode with modified characteristic (DMOD2). The 11 femto-farad parallel capacitor represents the parasitic capacitance of the bond pads.