B1500A Semiconductor Device Analyzer

技術概要

Introduction

Recent demand for characterizing high to medium power devices on the new materials such as SiC and GaN, and Organic devices requires both high voltage and high current measurement capabilities. Unfortunately, conventional DC measurement techniques can create device self-heating that causes the measured device behavior to deviate from that exhibited under normal operating conditions. Accurate characterization of these types of high-power devices requires pulsed current (I) and voltage (V) measurements with short measurement times. Until recently, solutions for pulsed IV measurement are limited for relatively wide pulse width in precise measurement or lower accuracy in narrow pulse. The Keysight Technologies, Inc. B1514A 50 μs Pulsed Medium Current Source Monitor Unit (MCSMU), which is a one slot plug-in module for B1500A with minimum 50 μs pulse width and 30 V-1 A (0.1A DC) maximum voltage and current output capability, improves these situations and allows you to focus on your real goal: parametric measurement and analysis.

Key Features

Up to 30 V/1 A pulse

MCSMU can source 30 V and 1 A pulse into a load accurately. You can easily expand to new applications by just adding MCSMUs to your B1500A.

Min 50 μs pulse width with 2 μs resolution

You can improve the pulsed measurement with more than ten times narrower pulse width with the SMU technology. The minimum 50 μs/30 V pulse (min 10 μs programmable) enables the precision pulsed measurement with lower junction temerature which is closer to real operating condition.

Integrated voltage and current waveform monitoring capability for accurate pulsed measurement

You can further enhance your pulsed measurement accuracy by using new Oscilloscope View capability which can monitor both the output current and the voltage (IV) waveforms in minimum 2 μs interval. You can set the narrow pulses accurately and easily by optimizing the pulse timing parameters in real time by using this capability. The Oscilloscope View realizes the simultaneous current waveform monitoring in synchronize with the voltage waveform that is not easy even using an oscilloscope. The Oscilloscope View is available in the Tracer Test mode (Curve tracer operation), and you can monitor up to four waveforms.

Easy setup using Keysight EasyEXPERT software

Keysight EasyEXPERT software, included with the B1500A, is a powerful environment for device evaluation and data analysis. For pulsed IV measurements using the MCSMU modules, three application tests for high-power pulsed IV (Id-Vds MCSMU, Id-Vgs MCSMU, Id-Vgs MCSMU 2-stage) are available. Tracer Test mode includes several sample setups menu where you can start measurement sooner by interactively controlling the test.

Performance examples

Following demonstrates some of the pulsed IV measurement examples.

Oscilloscope view of 50 μs pulsed IV measurement

Figure 1 shows the drain pulse waveforms of ID-VGS measurement. In this example, the drain is set for 10 V/50 μs pulse and the gate is swept from 4 to 4.5 V (pulse base is 2 V) with 40 μs pulse. Oscilloscope View shown in figure 1 monitors VDS, ID and VGS at the VGS setting of 4.5 V with 10 μs delay. The measurement time window is shown in green bar. You can move the maker line at any measurement timing of the time scale and the data at the marker position can be read out in the marker readout area. The example shows the VGS, VDS and ID data in the marker readout area at the 48 μs timing of the pulse where ID can be read as 646 mA. In this way, you can set the pulse timing accurately between the channels, and obtain the accirate result easily by using Oscilloscope View.

Example of Pulsed Id-Vd and Id-Vg measurement

Figure 2 shows an example of pulsed ID-VDS measurements for 1 A and 30 V.

  • Id-Vd measurement is made using the Tracer Test mode with 170 μs drain pulse. The setup is made by using Tracer Test mode Sample setups.

Figure 3 shows an example of pulsed Id-Vgs measurements with wide Id measurement features even under the pulsed measurement.

  • The Id-Vg measurements cover a wide current range (Seven digits resolution from 100 nA to 1 A in the example)
  • This measurement uses Id-Vgs MCSMU 2-stage application test (refer to Figure 3(a)).
  • The measurement is made by combining two Id-Vg measurements inside the application test.