技術概要
The Keysight Technologies, Inc. new X-series signal generators are crafted to create RF signals capable of testing your very best devices and designs. They produce the signals you need—from simple to complex, from incredibly
Boost every aspect of your test system performance
Wider frequency coverage, greater output power, and improved signal purity and modulation performance
More Applications
Analog and vector models offer a much wider range of signal simulation capabilities to test the latest generation of devices and receivers
Maximize Uptime
Enjoy the benefits of high reliability, maintainability, and a three year calibration cycle
More Compatibility
Achieve seamless migration and reduce transition risks
Overview: 8648A/B/C/D and the New EXG X-Series
Keysight 8648A/B/C/D signal generators were a very popular family of RF sources sold between 1996 and 2008. They were widely adopted for use in many RF signal generation applications, especially in manufacturing environments. The 8648-Series were known for providing excellent value with solid RF specifications and versatile capabilities, coupled with a proven track record of reliability. Because transitioning to a new signal generator requires careful consideration, this document was created to provide an overview of the new Keysight X-Series N5171B and N5172B EXG RF signal generators and a comparison of them with the 8648-Series sources.
Though the 8648-Series signal generators have been discontinued, Keysight will continue to provide full repair and calibration support services until March 2013. Beyond that date, support will be offered on a best-effort basis, and some users will elect to continue using their 8648’s for quite some time. However, new technologies and measurement demands will require higher levels of performance and greater certainty with respect to support services. Also, many users will prefer the latest instrument connectivity interfaces such as Gigabit LAN and dual USB ports. If these aspects interest you, then now is the time for you to make the transition from the 8648-Series to the new EXG.
何をお探しですか?