How to Pass RX Test According to PCIe 3.0 CEM Specifications

アプリケーションノート

Since the release of the PCIe® base specification revision 3.0 (rev. 3.0) in November 2010, many semiconductor vendors have tested their bare ASICs accordingly. Now PCIe 3.0 add-in cards (AICs) and motherboards (MBs) with PCIe 3.0 slots are being developed. These items need to be tested according to the PCIe Card Electromechanical (CEM) Specification, for which the Serial Enabling Group (SEG) is currently generating the PHY Test Specification.