Streaming Field Test with Task Planner

アプリケーションノート

Introduction

Ensuring the peak performance of RF systems has grown increasingly complex. In the field, RF issues like faulty transmitters and antennas, amplifier overdrive, and signal interference, can impact the operation of an RF system and result in degraded system performance. In addition, the rapid development of various RF systems (such as cellular, satellite, broadcasting, or military-related), means today’s field engineers and technicians also need to run routine tests and troubleshoot a larger array of systems.

This application note looks at the unique test equipment requirements of RF field engineers and illustrates how the new Task Planner feature of Keysight’s N9344C, N9343C, and N9342C handheld spectrum analyzers (HSAs) helps streamline system test and maximize RF network performance.