PS-X10-100 Web Remote Control Software for the MXA-N9020A, EXA-N9010A, Series Spectrum Analyzers - T

技術概要

Remote Control Over the Internet

The BenchLink Web Remote Control software is a utility that en­ables users to remotely control PSA, ESA-E, ESA-L series spectrum analyzers, and E7400A series EMC analyzers over the Internet or your company Intranet1. On the analyzer side, the instrument is connected to a local server computer via a GPIB or a LAN inter­face. The server computer must be connected to the Internet/Intranet. Multiple users can simultaneously access the analyzer from anywhere in the world by using a client computer connected to the Internet/Intranet. No special software is needed on the client side other than a standard web browser such as Microsoft Internet Explorer or Netscape Navigator.

Applications

The BenchLink Web Remote Control software is very useful in any application requiring remote viewing and control of the spectrum analyzer.

Signal Monitoring

Regulatory agencies and service providers must often monitor frequency bands to insure the quality and integrity of wireless communication systems. With the BenchLink Web Remote Control software, remote operators can monitor and document activity using a variety of displays – the standard spectrum analyzer

display, a “waterfall”, a “spectrogram”, an “analog+” or a

“persistence” display.

CATV Monitoring

CATV fiber hubs are typically situated in scattered locations throughout a city. Save valuable time by installing spectrum analyzers at hub sites and antenna sites, and monitoring activity over the network. The “analog+” display enables both field and manufacturing TV engineers to visualize and document transmitter intermodulation performance and AM linearity.

Satellite Earth Station Monitoring

Monitor the performance of multiple satellite bands and/or differ­ent sites from one convenient location. The “persistence” display emulates a phosphorescent CRT, allowing the engineer to

confidently determine persistent signals from occasional ones.

Manufacturing Process Monitoring

Many electronic manufacturing processes run continuously 24 hours a day, 7 days a week. Engineers must often monitor the progress of a specific test at inconvenient hours. The BenchLink Web Remote Control software makes it possible to do this by using a laptop computer from home or while traveling.

Features

BenchLink Web Remote Control software provides direct control of the following spectrum analyzer functions:

  • start/stop frequency
  • center frequency/span/zero span
  • reference level
  • attenuator
  • resolution video bandwidth
  • video and power averaging
  • sweep time and number of sweep points
  • factory and user presets
  • preferences such as auto align on/off, IF auto ranging on/off
  • global auto couple on/off
  • markers
  • detectors