白書
The dual-Dirac model is a tool for quickly estimating total jitter defined at a low bit error ratio, TJ(BER). The deterministic and random subcomponents of the jitter signal are separated within the context of the model to yield two quantities, root-mean-square random jitter (RJ) and a model-dependent form of the peak-to-peak deterministic jitter, DJ(δδ). The total jitter of a system is then estimated from RJ and DJ(δδ).
This paper provides a complete description of the dual-Dirac model, how it is used in technology standards and a summary of how it is applied on different types of test equipment. The Q-scale formulation is described in detail and is used to provide a simple visual description of the model’s features and to show how different implementations of the model can lead to different results. For an introduction to jitter analysis please see reference.
何をお探しですか?