Physics-Based Transformer Modeling for Power Converter Simulation

アプリケーションノート

Accurate transformer modeling is essential for reliable power converter simulation. In many traditional SPICE-based workflows, transformers are represented using linear inductors combined with ideal mutual coupling elements. While this approach is computationally efficient, it assumes constant permeability and linear magnetic behavior. In practice, ferrite cores used in power converters exhibit strongly nonlinear characteristics such as saturation, hysteresis, remanence, and bias-dependent permeability. These magnetic effects influence magnetizing current, core losses, waveform distortion, inrush behavior, and overall converter efficiency — making simplified linear models insufficient for modern high-performance designs.

 

Real magnetic materials do not follow a simple linear relationship between magnetic field strength and flux density. Instead, their behavior is described by nonlinear B–H hysteresis loops, where permeability varies with operating point, temperature, and DC bias conditions. As switching frequencies increase and converters operate closer to material limits, these nonlinearities become increasingly important to capture accurately in simulation.

 

To address these limitations, Keysight Advanced Design System (ADS) provides physics-based magnetic modeling capabilities using the Jiles–Atherton model. This model represents the physical behavior of magnetic materials and accurately reproduces hysteresis effects, including saturation, coercivity, remanence, and differential permeability variation. By incorporating material physics directly into the simulation environment, designers can predict magnetizing current, core losses, and nonlinear distortion effects with significantly greater accuracy than traditional linear models.

 

This application note demonstrates how to construct a nonlinear transformer model in ADS using the integrated Transformer Designer workflow. The example design is based on a U25/16/6 ferrite core with 3E27 ferrite material. The workflow shows how to extract key geometric and magnetic parameters from component datasheets, configure the nonlinear core properties using the Jiles–Atherton model, and automatically generate a transformer component suitable for circuit-level simulation.

 

The application note also illustrates how the generated transformer model can be validated and evaluated within a testbench environment. By simulating magnetizing current, nonlinear flux behavior, and waveform distortion, designers can observe the real operating characteristics of the transformer under switching conditions. This approach provides deeper insight into magnetic behavior that cannot be captured with simplified inductive representations.

 

For modern power electronics design — particularly in flyback, forward, and resonant converters — accurate magnetic modeling plays a critical role in predicting performance and ensuring robust operation. Physics-based transformer models improve confidence in simulation results, reduce the number of hardware design iterations, and enable more reliable prediction of efficiency, thermal behavior, and waveform integrity. By leveraging advanced magnetic modeling in ADS, engineers can bridge the gap between theoretical simulation and real-world magnetic component behavior.