Efficient Network Traffic Simulation Using HAR Files in BreakingPoint

アプリケーションノート

In Keysight Technologies BPS 9.22 software release for BreakingPoint System comes with a new feature called “HTTP Archive Record (HAR) Simulation” which empowers the users to create rapid simulation of web applications using any HAR capture file conforming to the HTTP Archive v1.2 specification (W3C standard). In this Application Note we will dive deep into HAR file format and how it can help to create rapid network traffic simulation strategies with Breakingpoint System.