Compliance Testing PCIe 5.0

白書

Data center operators need to embrace next-generation technologies to support the response times and high bandwidth requirements of 5G and IoT. With the expectation of billions of internet-connected devices and data-intensive real-time applications, 100 gigabit Ethernet (GE) speeds that are common in data centers today will not be fast enough. As a result, data center operators need to migrate their networks from 100GE to 400GE. Faster networking speeds require faster memory and faster serial bus communications.

In parallel with transceiver upgrades to 400GE, data center operators must transition to the next generation of high-speed computing interfaces. Double date rate (DDR) memory will move from DDR 4.0 to DDR 5.0, and Peripheral Component Interconnect Express (PCI Express® or PCIe®) expansion bus will move from PCIe 4.0 to PCIe 5.0.