Next-Generation Firewall 600 Gbps Throughput Test

レポート

Palo Alto Networks PA-7080 Validated with Ixia CloudStorm 100GE

 

Executive Summary

 

Ixia, a Keysight Business engaged with Palo Alto Networks to validate a fully loaded PA-7080 next-generation firewall (NGFW) with the latest 100G-capable network processing cards using Ixia’s CloudStorm 100GE, the flagship application and security test solution.

 

The PA-7080 enables the highest levels of performance while maintaining industry-leading security effectiveness. This is especially true with the release of the brand-new network processing card (NPC), which increases performance metrics over their first-generation by several folds. Alongside the PA-7080’s ability to linearly scale in terms of performance as NPCs are added to the chassis, this solidifies the 10-slot PA-7080 as the fastest NGFW on the market.

 

CloudStorm simulates 2.4 terabits of mixed applications, as well as malicious traffic, to test the critical elements of complex data centers, including server applications, storage workloads, and network security devices. As a result, it can validate the efficacy of the application and threat detection engines of NGFWs, measure the impact of SSL traffic on performance, and assess distributed denial of service (DDoS) mitigation techniques. This enables our mutual customers to validate the performance of their hyperscale data centers, while improving the security resiliency of their network.