How to Test Virtual VNF

白書

Top Five Lessons Service Providers Learn on Their Quest to Deploy a Virtualization Solution at Peak Performance

Until recently, network functions virtualization (NFV) was confined to development (dev) teams in the lab. However, service providers have begun moving functions from the lab to production. Now, they must make sure virtual network functions (VNFs) can perform optimally within a platform like OpenStack. Network monitoring and service assurance teams are tasked with deployment. Their challenge is to successfully deploy, integrate, and operate the slew of VNFs coming out of the dev lab. But without the right testing and monitoring, deployments can fail and the costs can go beyond money.