Article Reprints
Introduction
The paradigm shift ushered in by 6G will require innovating testing approaches that can adapt to the evolving definition of “next-next-generation.”
Mobile providers are accelerating their rollout of the flexible, low-latency, multi-gigabit-persecond communications network known as 5G. The technology promises to deliver not just faster data rates, but a more flexible and programmable network. This will be combined with the high reliability and low latency required to create secure, reliable wireless ecosystems to benefit industries beyond traditional smartphone use-models like manufacturing, transportation, and healthcare.
As many of us are just becoming familiar with the benefits of 5G, technology and communications companies are looking ahead to the next generation, 6G. Although the actual job description of 6G is still being written, the hopes for the technology are to enable a pervasive, seamless internet of things that connects not only people’s devices to the network, but allows sensors, vehicles, and many other products and technologies to communicate with each other seamlessly and reliably. For example, having vehicles that can not only communicate to the cloud, but to each other will result in more efficient traffic and safer travel, proponents say.
The differences between 5G and 6G are not just about what collection of bandwidths will make up 6G in the future and how users will connect to the network, but also about the intelligence built into the network and devices. “The collection of networks that will create the fabric of 6G must work differently for an augmented reality (AR) headset than for an e-mail client on a mobile device,” says Shahriar Shahramian, a research lead with Nokia Bell Laboratories. “Communications providers need to solve a plethora of technical challenges to make a variety of networks based on different technologies work seamlessly,” he says. Devices will have to jump between different frequencies, adjust data rates, and adapt to the needs of the specific application, which could be running locally, on the edge of the cloud, or on a public service.
“One of the complexities of 6G will be, how do we bring the different wireless technologies together so they can hand off to each other, and work together really well, without the end user even knowing about it,” Shahramian says. “That handoff is the difficult part.”
Although the current 5G network allows consumers to experience more seamless handoffs as devices move through different networks—delivering higher bandwidth and lower latency— 6G will also usher in a self-aware network capable of supporting and facilitating emerging technologies that are struggling for a foothold today—virtual reality and augmented reality technologies, for example, and self-driving cars. Artificial intelligence and machine learning technology, which will be integrated into 5G as that standard evolves into 5G-Advanced, will be architected into 6G from the beginning to simplify technical tasks, such as optimizing radio signals and efficiently scheduling data traffic.
“Eventually these [technologies] could give radios the ability to learn from one other and their environments,” two Nokia researchers wrote in a post on the future of AI and ML in communications networks. “Rather than engineers telling … nodes of the network how they can communicate, those nodes could determine for themselves—choosing from millions of possible configurations—the best possible to way to communicate.”
O que você está procurando?