Solution Briefs
PROPSIM FS16 5G Channel Emulation Solution
End-to-end real-world performance testing for wireless devices and base stations in the lab
The latest advancements in commercial wireless technologies address high-density environments like trains, stadiums, and airports. They require 3D spatial beamforming, multi-user massive multiple-input multiple-output (MU-MIMO), and more advanced spectrum utilization to increase wireless RF propagation channel effectiveness between devices and base stations.
With 5G devices, the data speed experienced by the user is highly dependent on the performance of the device in harsh mobile environments. Keysight’s family of 5G channel emulators are widely used by the industry to benchmark and validate devices and base stations end-to-end real-world performance in the lab environment.
O que você está procurando?