Case Studies
LEADING FRENCH TELECOM PROVIDER ENHANCES VISIBILITY AND TROUBLESHOOTING
Bouygues Telecom is a leading French mobile phone, Internet service provider, and IPTV company. Headquartered near Paris, Bouygues Telecom depends on a network of more than 10,000 devices to power a wide variety of services for its customers.
To stay competitive, Bouygues Telecom needs to deliver consistently superior performance for its end users, as well as dependable operation. But keeping its large, complex network running at its best was a challenge. Real-time Internet services can be seriously impacted by bottlenecks and other hard-topinpoint issues in the network. The provider also lacked the tools and visibility it needed for insight into the health of its network.
“We needed a better way to summarize the performance of our network in one dashboard,” says Adrien d’Ussel, Head of IP Network Performance at Bouygues Telecom. “We also wanted to make it easier to detect performance issues before they could impact our customers. And we required better testing to detect and troubleshoot potential problems on our network.”
D’Ussel adds, “The Hawkeye™ solution enables us to perform a diverse array of tests, which is very useful. It also enables us to aggregate our test results to provide better insight into the health of our network infrastructure, all in one view.”
DELIVERING IN-DEPTH MONITORING AND TESTING
To gain the insight it required, Bouygues Telecom deployed Hawkeye, the industry’s leading network and application assessment tool.
Hawkeye makes it easy for Bouygues Telecom to assess and troubleshoot its network and applications before and after deployment. Designed specifically for IT and Telecom teams, the solution enables organizations to confidently assess the performance and reliability of applications running on wired, wireless, and virtual data centers. With Hawkeye, Bouygues Telecom operations teams can capture network diagnostics virtually anywhere, using a web browser.
A COMPLETE SOLUTION SPANNING THE ENTIRE NETWORK
Bouygues Telecom deployed its Hawkeye management virtual server in its secured data center. It also deployed XR2000™ Active Monitoring Probes in different network locations on physical and virtual devices. These hardware and software probes enable assessment and monitoring of network and application performance in only two clicks.
Every 15 minutes, the organization’s probes launch Internet Control Message Protocol (ICMP) ping tests across 7,000 devices spanning its entire mobile network. The probes also regularly monitor access to the 3,000 devices in Bouygues Telecom’s fixed access network.
Bouygues Telecom chose Ixia’s solution based on Ixia’s deep technical experience in testing, and its ability to support softwarebased network monitoring. Ixia software was flexible enough to accommodate specific requirements for the Bouygues Telecom data model and also fit an integration of the data with the existing data mining infrastructure.
Ixia worked closely with Bouygues Telecom to maximize the solution’s scalability and upgrade its data model to obtain the best possible performance to get quick access to the vast amount of data points provided. Ixia also optimized the Hawkeye filters to boost results and enable fine granularity investigation of network performance.
O que você está procurando?