eBooks
The Intelligent Car is Here
The automotive industry is accelerating its electronic technology revolution and fusing with the clean energy ecosystem. By 2030, 4.2 million cars will be autonomous and 50% will be electric.
Dramatic increases in the number of sensors and applications in new automobiles have evolved the vehicle from a peripheral role to a network hosting clusters of connected devices. Cars now need to be optimized for:
• power efficiency
• sensor fusion
• communications
• high-power processing
• high throughput data connectivity
O que você está procurando?