5G Waveform Evaluations – mmWave Communication with SystemVue

Notas de Aplicação

Due to the potential availability of enormous channel bandwidths, the millimeter wave (mmWave) bands are currently being eyed for mobile radio communications. Larger channel bandwidths are critical to enabling the wireless industry to meet the increasing data rate and capacity demands of future wireless networks. One of the key issues in the radio interface design for mmWave communications is the selection of waveform. A key challenge; however, is that at high carrier frequencies, e.g. mmWave bands, transmitted and received signals can suffer from severe hardware impairments. Evaluating the performance of several stateof-the-art waveforms in the presence of hardware impairments is therefore of great importance to proper waveform design.