Notas de Aplicação
As this application note explains, understanding the type of jitter, its component characteristics, and measurement vantage points can help engineers identify its causes and diminish its effects on circuits and products.
Introduction
Jitter refers to how early or late a signal transition is compared with the time it should transition. This applies whether the time reference comes from the sampled data or an outside source. Transmission errors can occur when jitter causes a signal to be on the “wrong side” of the transition threshold at the sampling point. Therefore, causing the receiving circuit to interpret that bit differently than the transmitter intended (see Figure 1).
Table of Content
Sources of Jitter
Jitter on a signal will exhibit different characteristics depending on its causes. Thus, categorizing the sources of jitter is important. The primary phenomena that cause jitter are as follows:
System phenomena
These are effects on a signal that result from it being a digital system in an analog environment. Examples of these system-related sources include the following:
Data-dependent phenomena
These are patterns or other characteristics of the transferred data that affect the net jitter arriving in the receiver. Data-dependent jitter sources include the following:
Random noise phenomena
Some jitter phenomena randomly introduce noise in a system. These sources include the following:
These phenomena occur in all semiconductors and components. You will encounter them in phase-locked-loop designs, oscillator topologies and designs, and crystal performance.
O que você está procurando?