Port Setup Using ADS Momentum and Modelithics Models

Notas de Aplicação

A good understanding of proper EM port setup, configurations and calibration types is required to ensure accurate EM-circuit co-simulation results. This paper is intended to help users of Keysight Technologies’ Advanced Design System (ADS) and Modelithics models, accurately and efficiently simulate RF and microwave circuits. The focus of this paper is on finding the optimum port setup for EM simulation of circuit layouts that include surface mount devices and is organized into 3 main areas.

The first area provides detailed information concerning Momentum port types and calibration definitions and what you need to know with differential port configuration. Next is the results section, which includes examples that provide insight into port, momentum port calibration types and calibration performance. The final section contains the recommended calibration type and port configurations tips when using Modelithics models in co-simulations.  Download this excellent ADS Momentum and Modelithics Models guide today.