Notas de Aplicação
The DDR libraries available are written with the assumption that all the pins are connected to a boundary scan cell. In a real board application however, there are pins that are not connected to boundary scan cells, in which case we will need to modify the DDR library to generate the silicon nail test.
O que você está procurando?