Temperature Gauge with Multimeter DC Power Supply (U3606B)

Notas de Aplicação

Temperature plays an important role in maintaining the overall functionality of an electrical appliance and the design of these controller circuits is getting increasingly stringent. This makes it important to test the integrity of components and the overall the controller circuit. This article illustrates the unique features of the Keysight Technologies, Inc. U3606B multimeter | DC power supply that can be used to evaluate the functionality of a temperature controller board.