Notas de Aplicação
Electrical pulses are used to synchronize, trigger or control multiple electrical devices in a test system. Pulses are also used for clock generation or radar testing. In order to describe a pulse and make its creation repeatable, a set of parameters has been defined. This document describes and illustrates all main pulse parameter definitions. It is a collection of terms used in the test and measurement environment. The information will help the reader to understand the nature of a pulse, and will make instrument specifications comparable amongst each other.
O que você está procurando?