Conducting Site Surveys Using Handheld Spectrum Analyzers

Notas de Aplicação

Introduction

Rapid expansion of wireless services, consumer expectations and needs, and the complexity of wireless communication signaling approaches have brought huge value. But with that value the evolution has led to spectral crowding, difficulty in deploying new services, and higher potential for interference. These factors have made site surveys a necessity in a range of industries including military, medical, regulatory agencies, and wireless service providers.

Fortunately, technological advances in instrumentation have progressed along with the evolution of wireless communication. As this paper explains, those new technologies have allowed the development of progressive handheld spectrum analyzers (HSAs) such as Keysight Technologies N934xC family, which includes the 20 GHz N9344C, the 13.6 GHz N9343C, and the 7 GHz N9342C. These HSAs are easily capable of meeting the requirements of modern site surveys which has not always been the case with site survey equipment used in the past.