How to Use Keysight PXI Switches with NI Switch Executive

Notas de Aplicação

Managing switch paths in large test plans can be challenging. DUT’s that have high pin count or multiple-up configurations may require hundreds of individual paths during the course of a test plan. Switch executives can be very helpful when controlling a large number of switch paths. National Instruments Switch Executive uses information contained in the IVI switch driver to create and control valid paths for the switch. Keysight PXI switches are provided with IVI drivers, and as such can be used with the National Instruments Switch Executive (NI Switch Executive). The steps outlined in this application note provide a getting started guide for using Keysight’s PXI switches with NI Switch Executive.