Identifying an Electrical Circuit with Remote Connectivity

Notas de Aplicação

Introduction

Troubleshooting electrical circuits in an industrial environment can be difficult and hazardous. Sometimes, this troubleshooting task can lead to extended equipment outages, increased costs of repairs, and lost revenue. Commercial or residential electricians often need to identify the correct circuit breaker before commencing troubleshooting tasks. This is a time consuming and incredibly frustrating task. Electricians must also identify all loads connected to the same circuit, since the electrical panel’s labeling may not be adequate or correct. This application note explains how the Keysight Technologies, Inc. wireless remote connectivity solution helps to accelerate electrical circuit troubleshooting.

Methods to Identify an Electrical Circuit

Without proper labeling at the circuit breaker box or service panel, electricians first have to turn off each suspect circuit breaker in succession to identify the right electrical circuits.