Deploying Medalist i1000D ICT Tester with Board Handler

Notas de Aplicação

The Keysight Technologies, Inc. Medalist i1000D in-circuit test (ICT) system is a revolutionary platform with superior price-performance offerings. It comes with award winning state-of-the-art features to answer most test challenges faced by today’s manufacturers. Advanced limited access test features, coupled with a simplified, automated software model, shortens the learning curve of new users. Field evaluations have demonstrated that the i1000D delivers the fastest ramp up of test coverage among all similar-category testers.

 

As the pressure to lower labor costs continues, improving quality and increasing throughput, as well as automation in the SMT lines have become hot topics. The i1000D can now be deployed with board handlers to provide electronics manufacturers with even greater ease of use and flexibility in their automated in-circuit test strategy. Coupled with low-cost fixturing requirements and superior signal quality, these result in significant improvements in throughput, coverage and cost savings for electronics manufacturers.