E5071C ENA Series Network Analyzer

Folhetos

Procedure overview

  • Connect DUT to E5071C
  • Preset system and launch setup wizard
  • Configure E5071C with setup wizard VBA

In this demo guide, we will use BPF (Center frequency = 947.5 MHz), but you can use another filter. Prepare appropriate cable and adapter to connect between ENA and DUT.

1. Connect DUT to E5071C

Figure 1. DUT connection

In this demo, we will use 4-port E5071C. However, you can do the same demo with 2-port E5071C.

Legend: [Key name] = front panel hardware key

 Key name = soft key

 Number = front panel hardware numeric key

2. Preset system and launch setup wizard

3. Configure E5071C with setup wizard VBA

a. Press [Macro run] and wizard window is shown (Figure 2).

Additional Demo2: Analyze measurement result

  • To scale measurement result, press [Scale], then

Auto Scale or Auto Scale All

  • To search Maximum point, press [Marker Search],

then Max

  • To search Minimum point, press [Marker Search],

then Min

  • To search peak, press [Marker Search], then peak,

then Search peak

  • To show statistics, press [Marker Fctn] then turn on

Statistics

  • To change the trace, press [Trace Prev] or

[Trace Next]

  • To maximize or minimize the trace, press [Trace Max]