Notas de Aplicação
Overview
Designers of power amplifiers (PAs) used in wireless communication infrastructure today face many unique challenges, not the least of which is characterizing and modeling the component’s linear and nonlinear behavior. Complicating this task are long-term memory effects that make describing the PA characteristics, and therefore designing products with the PA, much more difficult.
What is a memory effect? Consider that a “memoryless” system is defined as y(t) = f(x(t)), where y(t) is the output signal, x(t) is the input signal and f is a linear or nonlinear function. Here, the output at any time depends only on the input signal value at that particular instant. In a system that has memory, this does not hold true. The output at a given time can depend not only on the present input value, but also previous output and input values. Common symptoms that let the designer know a system has memory are when the amplifier’s measured intermodulation distortion (e.g., TOI or IM3) changes as a function of the frequency difference between the two stimulus tones, its IM3 upper and lower sidebands exhibit asymmetry, or it produces hysteretic/multi-valued AM-AM and AM-PM amplifier responses in response to modulated signals.
O que você está procurando?