Debugging Serial Bus Systems with Infiniium Oscilloscopes

Notas de Aplicação

The Keysight Technologies, Inc. Ininiium Oscilloscopes provide many of the features of protocol analyzers such as decode listings and protocol speciic triggering. However, a good question is “If protocol analyzers already exist, why is this capability needed?”

First of all, having a single instrument that provides the capabilities of an oscilloscope, logic analyzer and protocol analyzer provides lots of advantages. First of all, there is the convenience of bench space. Why crowd your bench with three instruments when one will do? Secondly, even if you happen to have all three instruments handy, it is a hassle to turn on another instrument and set it up. A single “All-in-one” instrument saves time.