USB Multifunction DAQ U2331A in Construction Industry

Notas de Aplicação

The Keysight Technologies, Inc. U2331A data acquisition (DAQ) device can be used to measure various types of parameters in the construction industry. It is important for one to know the concept of the types of measurement needed in the industry, which this bulletin will touch on. People in the construction industry often test parameters such as pressure, strain, temperature, displacement, and force. By measuring the said parameters, engineers are able to determine if a structure will be able to withstand sudden changes in a normal operating environment, and estimate the degradation of certain construction materials, which are constantly used over a certain period. There is a distinct awareness of monitoring the integrity of such materials and their structure formation.