Notas de Aplicação
Voltage regulation is a crucial point to consider when one designs an electronics system. Voltage regulation can cause electronics system to become unstable and may cause system shutdown or failure.
The Keysight Technologies, Inc. U2351A data acquisition (DAQ) is used as an automatic DC voltage regulator in this application. The U2351A is used to induce voltage into the electronics system thereby causing an amount of under voltage or over voltage stress to the device under test (DUT). Therefore, when adding a certain plug-and-play device to the system, it is important to know if the DUT can maintain stability if the voltage varies.
O que você está procurando?