5530 Dynamic Calibrator

Catálogos

This Sensor Hub provides the interface for the Keysight Technologies, Inc. E1737A Material Temperature Sensor and Keysight E1738A Air Temperature/Pressure/ Humidity Sensor used with the Keysight 5530 Laser Calibration System. These sensors monitor parameters in the environment of the device being calibrated to enable the laser system to calculate appropriate correction factors. The E1736A can accommodate multiple sensors of both types. The sensor hub interfaces with the system PC via a standard high-speed USB interface.