Brochures
DC power supplies are a fundamental component of almost every test system. Today’s complex automatic test equipment (ATE) systems must perform a variety of tests quickly, either to increase test system throughput or to tweak and optimize design performance. Each step in the test may have different power requirements, and the setup time for each step can significantly affect test throughput. Devices that are powered by multiple DC power supplies may require the test system to turn power on in a particular order to prevent problems with the device, such as latch-up or excessive current flow. Power sequencing is used when you need to control sequences such as the shut down of devices either in normal testing or because of a fault condition.
Snapshot: Testing Product Reliability
During the design validation process, one liquid crystal display (LCD) manufacturer needed to ensure its inverter would perform as expected. Company engineers executed thousands of on/off tests precisely sequenced within 1 ms over a temperature range to ensure the inverter did not shorten the life of the cold cathode fluorescent lamp (CCFL) backlight, one of the key components of a LCD screen. The manufacturer was using multiple pieces of equipment in a costly, unreliable test system. To improve the reliability of the test, the manufacturer turned to the N6700 modular power system and modules to configure four synchronized outputs within a 1 U mainframe. Engineers used the delay feature to create precise power-on and power-off sequences and list mode to produce the pulse width modulation (PWM) for the digital dimming control signal. With the N6700, the manufacturer was able to reduce the test time and cost while improving reliability.
Power sequencing methods
You can use a number of methods to control the turn-on and shut-down sequence of multiple power sources. Using diodes between inputs or placing relays in series with the inputs introduces signal variations that interfere with the testing. Using software to control the sequence or relays in series with each input often results in imprecise timing.
Instruments such as Keysight Technologies, Inc. N6700 modular power system for ATE systems or the N6705A DC power analyzer for bench use makes it easy to set up sequences. Either of these mainframes can be configured with up to four power supply output modules out of more than 20 options to best fit your application needs.
To create turn-on and shut-down sequences using multiple sources, the delay feature can be used to specify the amount of time between the start of the sequence and the transition of each source.
List mode
You can make transitions between the turn-on and shut-down portions of your test. If your test requires a series of changes to the output level or a low frequency signal, you may face similar instrumentation and cabling challenges to setting up sequences, as well as investing the time and effort to configure it. Some power supplies have analog inputs that add external signals, such as a signal from a function generator, to the power output.
Fault conditions
Outputs can be sequenced off in response to a power supply fault event using the delay time settings. The supply output experiencing a fault event, such as over-voltage, over-current, or over-temperature, will shut down as quickly as possible to avoid damage to the device or the power supply. The remaining outputs will use the programmed delays for a controlled shut-down sequence. When you configure it to do so, the sequenced shut-down can be synchronized across multiple mainframes.
Summary
Creating power sequences for applications requiring multiple power outputs can help you run your tests reliably and prevent damage to your device. Power supplies with list mode can further reduce your test time by storing the series of changes in the instrument and eliminating the overhead of using programming commands. We have reviewed the benefits of list mode and synchronizing multiple power outputs to improve your test routine, and showed how Keysight’s N6700 and N6705A mainframes and modules makes it easy to include these features in your test.
O que você está procurando?